![]() |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
MIFARE RFID card reader design example
Description
NXP Semiconductors is the world leader in MIFARE contactless smartcard technology.
The software below is an example implementation of a contactless MIFARE reader with the Keil MCB2140 evaluation board featuring the LPC2148 Microcontroller and a connection to the NXP MFCR5xx chip and an antenna.
The code, while written for the LPC2148, will work with any member of the LPC213x, LPC214x, LPC23xx, or LPC24xx series with little-to-no modifications.
The example code/project for the LPC2148 uses our Basic Function Library (for NXP's MFRC500 and MFRC53x tranceiver ICs) to read ISO14443A part IV compliant contactless cards and is provided "as is" for reference only.
Please see the End User Licensing Agreement for terms and conditions.
Products
The following microcontrollers are compatible with the MIFARE RFID card reader design example:
MCUs
Click
MIFARE Reader ICsDemonstration and Evaluation BoardMore Information
End User License Agreement
Note: The EULA contains important license terms and contains the password to decrypt the example code below.
Example Code
Note: The example code above is encrypted and requires a password to access.
Disclaimer
This design example shows possible hardware and software techniques used to implement the design.
It is imperative that the viewer use sound engineering judgment in determining the fitness of this design example for any particular application.
This design example may include information from 3rd parties and/or information which may require further licensing or otherwise.
Additional hardware or software design may be required.
NXP Semiconductors does not support or warrant this information for any purpose other than an informational design example.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||