![]() |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Future Designs, Inc. Single-Chip LCD Demo (LCD-DEMO-SC)
Introduction
The LCD-DEMO-SC development tool is a single-chip solution for implementing an LCD user interface with the NXP LPC9408 along with a couple of discrete external components.
The board is controlled by a two-button user interface allowing you to control the 8-character alphanumeric LCD display.
A 128-segment PCF8562 I2C-based LCD driver is included on the board.
An on-board 10-pin header allows you to use any external ICP style programmer to edit and download source code to the reprogrammable flash microcontroller.
With the microcontroller's full 8KB of flash memory, the LCD-DEMO-SC can also function as a Single Board Computer with multiple I/O options supported by its 12-pin header.
The full kit includes the LCD demo board and a CD containing sample code, schematics, and ICP documentation.
Key Components
The demo board includes the following key components:
The NXP LPC9408 is a multi-chip module (MCM) made up of the following two devices:
When used as a Single Board Computer, the I/O expansion header provides access to:
Note: The LCD-DEMO-SC supports both the P89LPC9408 and the P89LPC9401.
![]() Front View
![]() Back View
DocumentationProducts
Supported Products
Click
Vendors
Obtaining the Demo Board
More Information
Manufacturer Links
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||