![]() |
||||||||||||||||||||||||||||||||||||||||||||||||||||
|
||||||||||||||||||||||||||||||||||||||||||||||||||||
Future Designs, Inc. Socket Adapter Boards for USB In-System Programmer for LPC2000 (SAB-TFBGAxxx)
Introduction
The SAB-TFBGAxxx Socket Adapter Boards extend the capability of the popular USB In-Circuit Programmer for NXP's LPC2000 microcontrollers.
These boards allow you to program and test LPC2000 microcontrollers outside of their application circuit and before prototype boards are available.
The SAB-TFBGAxxx can also be used for verification of basic functionality of the user software as the board may be used completely stand-alone.
The SAB-TFBGAxxx comes with the adapter board, power supply, and RJ45 Ethernet-style cable.
The SAB-TFBGAxxx Socket Adapter Board plugs directly into the USB In-System Programmer for LPC2000 microcontrollers via the ethernet cable, and thus requires the USB-ICP-LPC2K.
Key Components
The adapter board has the following key components:
![]() DocumentationProducts
Supported Products
Click
The SAB-TFBGA100 supports the following microcontrollers:
The SAB-TFBGA180 supports the following microcontroller:
The SAB-TFBGA208 supports the following microcontrollers:
Vendors
Obtaining the Adapter BoardMore Information
NXP Links
Manufacturer Links
|
||||||||||||||||||||||||||||||||||||||||||||||||||||