![]() |
||||
|
||||
USB host mass storage class (MSC) example
Introduction
NXP Semiconductors and OnChip Technologies have partnered to provide USBHostLite software for our LPC1000, LPC2000, and LPC3000 families of microcontrollers with USB host capability.
These include members of the LPC17xx series, the LPC23xx series, the LPC24xx series, the LPC29xx series, the LPC31xx series, and the LPC32xx series of microcontrollers.
USBHostLite is a stripped-down USB host stack that includes only USB mass storage class support with the bare minimum code to run in an OS-less environment.
USBHostLite provides a simple solution for accessing the files on USB mass storage devices such as USB Pen Drives, USB Hard Disk Drives, etc., connected to the USB Host port.
Features
The USBHostLite supports the following features:
Limitations
The complimentary USBHostLite software from NXP has following limitations:
Note: This application note describes the USBHostLite stack in general and its application on the Embedded Artists LPC2468 OEM board in particular.
Software
USBHostLite for LPC source code is free to NXP customers for unlimited use with NXP LPC2000 and LPC3000 families of microcontrollers only.
By downloading or using the USBHostLite software, you agree to use it solely with these NXP microcontrollers.
USBHostLite stack ported to the LPC293x devices on the Hitex LPC2939 board:
USBHostLite stack ported to the LPC2468 device on the Embedded Artists LPC2468 OEM board:
USBHostLite stack ported to the LPC1768 device on the Keil MCB1760 evaluation board:
For customer applications requiring full featured and production quality embedded USB stacks, OnChip Technologies LLC provides embedded USB Host/Device/OTG stacks that are fully compliant with the USB specifications and offers great degree of stability and configurability.
More Information
Disclaimer
This software is provided AS-IS by NXP Semiconductors.
NXP Semiconductors does not support or warrant the software contained herein for any purpose other than for informational use.
Please contact OnChip Technologies LLC for further assistance including support options and other embedded USB host/device/OTG stacks.
For Further AssistanceOther Professional USB Host Stack Solutions for the LPC3000, LPC2000, and LPC1000 families |
||||